Part Number: TMS320F28379D
Hi der people,
by my application I need to generate two interrupts per ePWM-Period. The one on TBCTR = CMPA, the other on TBCTR = CMPB.
Now, if I understood correctly, when I set
EPwm2Regs.ETSEL.bit.INTSELCMP = 0; // Enable event time-base counter equal to CMPA or to CMPB when the timer is incrementing to INTSEL selection mux.
EPwm1Regs.ETSEL.bit.INTSEL = 100; // 100: Enable event time-base counter equal to CMPA or CMPC when the timer is incrementing
I would get an interrupt on CMPA
This means, if I also want an interrupt on CMPB I need to change the register inside the interrupt routine to this :
EPwm1Regs.ETSEL.bit.INTSEL = 110; // 110: Enable event: time-base counter equal to CMPB or CMPD when the timer is incrementing
And set it back by the next inerrupt to
EPwm1Regs.ETSEL.bit.INTSEL = 100;
Is there another way I am overlooking?
Thanks and best regards!
Gustavo