This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For a given device/HRPWM instance, at fixed voltage and fixed temperature, what is a rough ballpark for typical HRPWM MEP step size variance? Using SFO, we will have an average step size, represented as a number of steps per one sysclk tick. Understand that this is not a characterized data manual parameter, just trying to get a rough understanding of what to expect, i.e. +/- 10%, 20%, 40%? The use case is understanding the absolute delay of say 5 to 10 steps. If the average value is used, what would be a decent rule of thumb for the error (using SFO based average)?
A side question would be related to voltage sensitivity. Can a change from 1.2 to 1.15V have a significant impact? This relates to the assumption of fixed voltage.
HI Nima,
Thanks for digging up this info. +/- 2% is pretty tight (better than expected tolerance over all process corners). I assume that this step to step variance is independent of the SFO "average" effect?
For example, if SFO comes back with 33 steps/Sysclk (10nS), the average is 303pSec. If SFO comes back with 34 steps/Sysclk tick, the average is 294pSec. At this end of the range, the SFO average number will be roughly +/- 1.5%.
Is the +/-2% number exclusive or inclusive of the SFO average error? In other words, is the +/-2% based on actual process data and not based on the usage of a SFO determined average step size (as would be used in the actual application)?
Is the +/-2% based on design simulation data?
Regards,
Eric