This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Merry Christmas experts,
Customer found unexpected GPIO26 toggling on 100pin F280049 during EMC test, even without any change on GPIO26's "data", "clear", "set" or "toggle" register.
They have inserted some code to check GPADAT.bit.GPIO26 and this bit is changed even without intended change. Finally, they found "GpioDataRegs.GPADAT.bit.GPIO25 = 0" in ISR caused this problem, after they changed to "GpioDataRegs.GPACLEAR.bit.GPIO25 = 1", GPIO26 will not have any problem any more.
Could help me with any explanations or suggestions?
Thanks
Sheldon