hi Sir/Miss,
Does anyone know what to do if my crystal amplitude does not meet C2000 min VIH (VDDIO x 0.7)?
If Worst Case VDDIO = 3.37V, Minimum VIH to be recognized by C2000 is 3.37V x 0.7 = 2.359V.
But the max peak 20MHz crystal oscillation X1 (input to C2000) below has typical 2.29V. So it failed to meet VIH.
May I reduce the crystal capacitance load, CL ? Currently it is 18pF for both X1 and X2 end as per C2000 datasheet recommendation.
Shall I reduce to about 12pF to check if the VIH can be met?
Thanks for your advice in advance.