Part Number: LAUNCHXL-F28027
Hello, I'm using the C2000 support package for Matlab with my F28027F launchpad. Now I'm testing a current sensor (LA25-np). I used the ADC block to read the analog value from the sensor. All settings of the ADC block are left intact. Unfortunately, there is a lot of noise in the reading I got. Attached image below is the scope reading directly taken from the ADC block. Is there any setting that I'm not aware of regarding this issue?
Then, I tried to read the output from the same sensor using my Arduino Uno with Arduino support package for simulink just to double check. The reading is good as can be seen below.