This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using the F280049 controlCARD Installed on TMDSHSECDOCK with Code Composer Studio Version: 9.1.0.00010 .
I made some tests with the ePWM peripheral. I'm using the up&down mode and the CMPA to generate PWMA. This signal is used to generate PWMA&PWMB with the deadband module. The deadband module is running at half cycle.
So I generated a PWM and his complement with the deadband module. I could easily modify the duty cycle (CMPA register) and the deadtime (DBRED/DBFED registers). The duty cycle has 10ns resolution and the deadband 5ns.
Then I tried to use the High Resolution capabilities of the ePWM. Without using the deadband module, I could generate a HRPWM and modify the duty cycle easily. But I didn't succeed to generate a HRPWM with the deadband module. It seems that the deadband module keep the 5ns resolution. I used the deadband in High Resolution with a deadband of 100ns so DBREDHR & DBFEDHR registers are set to 0.
A workaround has been:
However, I missed something and I would like to understand what I missed.
Could you confirm to me that it's possible to use High resolution capabilities on duty cycle with the deadband module? If yes, is there some specific configurations, tricks, ... to know? is there an example available using HRPWM for duty cycle with the deadband module?
Thanks for your next answers
Yes aboslutely you can use deadband module with HR along with the duty HR.
We actually have an example for this:
http://dev.ti.com/tirex/explore/node?node=AO-6xsLBZFHVI45MT.pHCQ__gYkahfz__LATEST
Thanks, I have to explore more in detail this example and test it. After a first look, I didn't found the difference with my software!!!
I will keep you inform of the result.
best regards,
Yann