This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am trying out a simple workflow for F2838x ControlCard checking the GPIO pins. In this case I have used external jumper and shorted GPIO10 and GPIO12. In the code I am configuring GPIO10 as input and GPIO 12 as output. I will set the value of GPIO12 and read the data from GPIO10 immediately to a variable. Here is the code I am using.
//########################################################################### // // FILE: gpio_ex1_setup.c // // TITLE: Device GPIO Setup //! <h1> Device GPIO Setup </h1> //! \addtogroup bitfield_example_list //! //! Configures the F2838X GPIO into two different configurations //! This code is verbose to illustrate how the GPIO could be setup. //! In a real application, lines of code can be combined for improved //! code size and efficiency. //! This example only sets-up the GPIO. //! Nothing is actually done with the pins after setup. // //############################################################################# // $TI Release: F2838x Support Library v2.00.00.03 $ // $Release Date: Sun Sep 29 07:45:41 CDT 2019 $ // $Copyright: // Copyright (C) 2019 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // Included Files // #include "f28x_project.h" // // Defines // Select the example to compile in. Only one example should be set as 1 // the rest should be set as 0. // #define EXAMPLE1 0 // Basic pinout configuration example #define EXAMPLE2 0 // Communication pinout example // // Function Prototypes // void setupGPIOLoopBack(void); void setup1GPIO(void); void setup2GPIO(void); Uint16 InputValue = 0; Uint16 OutputValue = 0; // // Main // void main(void) { // //Step 1. Initialize System Control: //PLL, WatchDog,enabe Peripheral Clocks //This example function is found in the f2838x_sysctrl.c file. // InitSysCtrl(); // //Step 2. Initialize GPIO // InitGpio(); // //Step 3. Clear all __interrupts and initialize PIE vector table: //Disable CPU __interrupts // DINT; // //Initialize the PIE control registers to their default state. //The default state is all PIE interrupts disabled and flags //are cleared. // InitPieCtrl(); // //Disable CPU interrupts and clear all CPU interrupt flags: // IER = 0x0000; IFR = 0x0000; // //Initialize the PIE vector table with pointers to the shell Interrupt //Service Routines (ISR). // InitPieVectTable(); // //Step 4. User specific code: // setupGPIOLoopBack(); #if EXAMPLE1 // //This example is a basic pinout // setup1GPIO(); #endif #if EXAMPLE2 // // This example is a communications pinout // //setup2GPIO(); #endif while(1) { //ESTOP0; InputValue = 1; if (InputValue == 1) GpioDataRegs.GPASET.bit.GPIO12 = 1; else GpioDataRegs.GPACLEAR.bit.GPIO12 = 1; OutputValue = GpioDataRegs.GPADAT.bit.GPIO10; DELAY_US(500000); InputValue = 1; if (InputValue == 1) GpioDataRegs.GPASET.bit.GPIO12 = 1; else GpioDataRegs.GPACLEAR.bit.GPIO12 = 1; OutputValue = GpioDataRegs.GPADAT.bit.GPIO10; DELAY_US(500000); InputValue = 0; if (InputValue == 1) GpioDataRegs.GPASET.bit.GPIO12 = 1; else GpioDataRegs.GPACLEAR.bit.GPIO12 = 1; OutputValue = GpioDataRegs.GPADAT.bit.GPIO10; DELAY_US(500000); InputValue = 0; if (InputValue == 1) GpioDataRegs.GPASET.bit.GPIO12 = 1; else GpioDataRegs.GPACLEAR.bit.GPIO12 = 1; OutputValue = GpioDataRegs.GPADAT.bit.GPIO10; } } void setupGPIOLoopBack(void) { // // Set GPIO10 as input and GPIO12 as output // EALLOW; GpioCtrlRegs.GPAPUD.bit.GPIO10 = 1; // Disable pullup on GPIO10 GpioCtrlRegs.GPAPUD.bit.GPIO12 = 1; // Enable pullup on GPIO12 GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 0; // GPIO10 = Input GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 0; // GPIO12 = Output // // Enable an GPIO output on GPIO12 // //GpioDataRegs.GPASET.bit.GPIO12 = 1; // Load output latch GpioCtrlRegs.GPADIR.bit.GPIO12 = 1; // GPIO6 = output GpioCtrlRegs.GPAQSEL1.bit.GPIO10 = 0; // asynch input GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 0; // asynch input EDIS; } // // setup1GPIO - Is an example that demonstrates the basic pinout // void setup1GPIO(void) { // // Example 1: Basic Pinout. // This basic pinout includes: // PWM1-3, ECAP1, ECAP2, TZ1-TZ4, SPI-A, EQEP1, SCI-A, CAN-A, I2C // and a number of I/O pins // These can be combined into single statements for improved // code efficiency. // // // Enable PWM1-3 on GPIO0-GPIO5 // EALLOW; GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0; // Enable pullup on GPIO0 GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0; // Enable pullup on GPIO1 GpioCtrlRegs.GPAPUD.bit.GPIO2 = 0; // Enable pullup on GPIO2 GpioCtrlRegs.GPAPUD.bit.GPIO3 = 0; // Enable pullup on GPIO3 GpioCtrlRegs.GPAPUD.bit.GPIO4 = 0; // Enable pullup on GPIO4 GpioCtrlRegs.GPAPUD.bit.GPIO5 = 0; // Enable pullup on GPIO5 GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = PWM1A GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO1 = PWM1B GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // GPIO2 = PWM2A GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // GPIO3 = PWM2B GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // GPIO4 = PWM3A GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // GPIO5 = PWM3B // // Enable an GPIO output on GPIO6, set it high // GpioCtrlRegs.GPAPUD.bit.GPIO6 = 0; // Enable pullup on GPIO6 GpioDataRegs.GPASET.bit.GPIO6 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 0; // GPIO6 = GPIO6 GpioCtrlRegs.GPADIR.bit.GPIO6 = 1; // GPIO6 = output // // Enable eCAP1 on GPIO7 // GpioCtrlRegs.GPAPUD.bit.GPIO7 = 0; // Enable pullup on GPIO7 GpioCtrlRegs.GPAQSEL1.bit.GPIO7 = 0; // Synch to SYSCLKOUT InputXbarRegs.INPUT7SELECT = 7; // INPUT7 = GPIO7 ECap1Regs.ECCTL0.bit.INPUTSEL = 7; // Select eCAP1 TO INPUT7 // // Enable GPIO outputs on GPIO8 - GPIO11, set it high // GpioCtrlRegs.GPAPUD.bit.GPIO8 = 0; // Enable pullup on GPIO8 GpioDataRegs.GPASET.bit.GPIO8 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 0; // GPIO8 = GPIO8 GpioCtrlRegs.GPADIR.bit.GPIO8 = 1; // GPIO8 = output GpioCtrlRegs.GPAPUD.bit.GPIO9 = 0; // Enable pullup on GPIO9 GpioDataRegs.GPASET.bit.GPIO9 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 0; // GPIO9 = GPIO9 GpioCtrlRegs.GPADIR.bit.GPIO9 = 1; // GPIO9 = output GpioCtrlRegs.GPAPUD.bit.GPIO10 = 0; // Enable pullup on GPIO10 GpioDataRegs.GPASET.bit.GPIO10 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 0; // GPIO10 = GPIO10 GpioCtrlRegs.GPADIR.bit.GPIO10 = 1; // GPIO10 = output GpioCtrlRegs.GPAPUD.bit.GPIO11 = 0; // Enable pullup on GPIO11 GpioDataRegs.GPASET.bit.GPIO11 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 0; // GPIO11 = GPIO11 GpioCtrlRegs.GPADIR.bit.GPIO11 = 1; // GPIO11 = output // // Enable Trip Zone inputs on GPIO12 - GPIO14 // GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0; // Enable pullup on GPIO12 GpioCtrlRegs.GPAPUD.bit.GPIO13 = 0; // Enable pullup on GPIO13 GpioCtrlRegs.GPAPUD.bit.GPIO14 = 0; // Enable pullup on GPIO14 GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 3; // asynch input GpioCtrlRegs.GPAQSEL1.bit.GPIO13 = 3; // asynch input GpioCtrlRegs.GPAQSEL1.bit.GPIO14 = 3; // asynch input InputXbarRegs.INPUT1SELECT = 12; // GPIO12 = TZ1 InputXbarRegs.INPUT2SELECT = 13; // GPIO13 = TZ2 InputXbarRegs.INPUT3SELECT = 14; // GPIO14 = TZ3 // // Enable SPI-A on GPIO16 - GPIO19 // GpioCtrlRegs.GPAPUD.bit.GPIO16 = 0; // Enable pullup on GPIO16 GpioCtrlRegs.GPAPUD.bit.GPIO17 = 0; // Enable pullup on GPIO17 GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0; // Enable pullup on GPIO18 GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0; // Enable pullup on GPIO19 GpioCtrlRegs.GPAQSEL2.bit.GPIO16 = 3; // asynch input GpioCtrlRegs.GPAQSEL2.bit.GPIO17 = 3; // asynch input GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3; // asynch input GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 3; // asynch input GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 1; // GPIO16 = SPISIMOA GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 1; // GPIO17 = SPIS0MIA GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 1; // GPIO18 = SPICLKA GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1; // GPIO19 = SPISTEA // // Enable EQEP1 on GPIO's 20,21,22,23 // GpioCtrlRegs.GPAPUD.bit.GPIO20 = 0; // Enable pullup on GPIO20 GpioCtrlRegs.GPAPUD.bit.GPIO21 = 0; // Enable pullup on GPIO21 GpioCtrlRegs.GPAPUD.bit.GPIO22 = 0; // Enable pullup on GPIO22 GpioCtrlRegs.GPAPUD.bit.GPIO23 = 0; // Enable pullup on GPIO23 GpioCtrlRegs.GPAQSEL2.bit.GPIO20 = 0; // Synch to SYSCLKOUT GpioCtrlRegs.GPAQSEL2.bit.GPIO21 = 0; // Synch to SYSCLKOUT GpioCtrlRegs.GPAQSEL2.bit.GPIO22 = 0; // Synch to SYSCLKOUT GpioCtrlRegs.GPAQSEL2.bit.GPIO23 = 0; // Synch to SYSCLKOUT GpioCtrlRegs.GPAMUX2.bit.GPIO20 = 1; // GPIO20 = EQEP1A GpioCtrlRegs.GPAMUX2.bit.GPIO21 = 1; // GPIO21 = EQEP1B GpioCtrlRegs.GPAMUX2.bit.GPIO22 = 1; // GPIO22 = EQEP1S GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 2; // GPIO23 = EQEP1I // // Enable eCAP1 on GPIO24 // GpioCtrlRegs.GPAPUD.bit.GPIO24 = 0; // Enable pullup on GPIO24 GpioCtrlRegs.GPAQSEL2.bit.GPIO24 = 0; // Synch to SYSCLKOUT InputXbarRegs.INPUT8SELECT = 24; // INPUT8 = GPIO24 ECap1Regs.ECCTL0.bit.INPUTSEL=8; // Select eCAP1 TO INPUT8 // // Set input qualification period for GPIO25 & GPIO26 // GpioCtrlRegs.GPACTRL.bit.QUALPRD3=1; // Qual period = SYSCLKOUT/2 GpioCtrlRegs.GPAQSEL2.bit.GPIO25=2; // 6 samples GpioCtrlRegs.GPAQSEL2.bit.GPIO26=2; // 6 samples // // Make GPIO25 the input source for XINT1 // GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 0; // GPIO25 = GPIO25 GpioCtrlRegs.GPADIR.bit.GPIO25 = 0; // GPIO25 = input GPIO_SetupXINT1Gpio(25); // XINT1 connected to GPIO25 // // Make GPIO26 the input source for XINT2 // GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 0; // GPIO26 = GPIO26 GpioCtrlRegs.GPADIR.bit.GPIO26 = 0; // GPIO26 = input GPIO_SetupXINT2Gpio(26); // XINT2 connected to GPIO26 // // Make GPIO27 wakeup from STANDBY Low Power Modes // GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 0; // GPIO27 = GPIO27 GpioCtrlRegs.GPADIR.bit.GPIO27 = 0; // GPIO27 = input CpuSysRegs.GPIOLPMSEL0.bit.GPIO27=1; // GPIO27 will wake the device CpuSysRegs.LPMCR.bit.QUALSTDBY = 2; // Qualify GPIO27 by 2 OSCCLK // cycles before waking the device // from STANDBY // // Enable SCI-A on GPIO28 - GPIO29 // GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0; // Enable pullup on GPIO28 GpioCtrlRegs.GPAQSEL2.bit.GPIO28 = 3; // Asynch input GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1; // GPIO28 = SCIRXDA GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0; // Enable pullup on GPIO29 GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1; // GPIO29 = SCITXDA // // Enable CAN-A on GPIO30 - GPIO31 // GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pullup on GPIO30 GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1; // GPIO30 = CANRXA GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pullup on GPIO31 GpioCtrlRegs.GPAQSEL2.bit.GPIO31 = 3; // Asynch input GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1; // GPIO31 = CANTXA // // Enable I2C-A on GPIO32 - GPIO33 // GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0; // Enable pullup on GPIO32 GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 1; // GPIO32 = SDAA GpioCtrlRegs.GPBQSEL1.bit.GPIO32 = 3; // Asynch input GpioCtrlRegs.GPBPUD.bit.GPIO33 = 0; // Enable pullup on GPIO33 GpioCtrlRegs.GPBQSEL1.bit.GPIO33 = 3; // Asynch input GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 1; // GPIO33 = SCLA // // Make GPIO34 an input // GpioCtrlRegs.GPBPUD.bit.GPIO34 = 0; // Enable pullup on GPIO34 GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0; // GPIO34 = GPIO34 GpioCtrlRegs.GPBDIR.bit.GPIO34 = 0; // GPIO34 = input EDIS; } // // setup2GPIO - Is an example that demonstrates the communications pinout // void setup2GPIO(void) { // // Example 2: // Communications Pinout. // This basic communications pinout includes: // PWM1-3, CAP2, SPI-B, CAN-A, SCI-A and I2C // and a number of I/O pins // // // Enable PWM1-3 on GPIO0-GPIO5 // EALLOW; GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0; // Enable pullup on GPIO0 GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0; // Enable pullup on GPIO1 GpioCtrlRegs.GPAPUD.bit.GPIO2 = 0; // Enable pullup on GPIO2 GpioCtrlRegs.GPAPUD.bit.GPIO3 = 0; // Enable pullup on GPIO3 GpioCtrlRegs.GPAPUD.bit.GPIO4 = 0; // Enable pullup on GPIO4 GpioCtrlRegs.GPAPUD.bit.GPIO5 = 0; // Enable pullup on GPIO5 GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = PWM1A GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO1 = PWM1B GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // GPIO2 = PWM2A GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // GPIO3 = PWM2B GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // GPIO4 = PWM3A GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // GPIO5 = PWM3B // // Enable an GPIO output on GPIO6 // GpioCtrlRegs.GPAPUD.bit.GPIO6 = 0; // Enable pullup on GPIO6 GpioDataRegs.GPASET.bit.GPIO6 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 0; // GPIO6 = GPIO6 GpioCtrlRegs.GPADIR.bit.GPIO6 = 1; // GPIO6 = output // // Enable eCAP1 on GPIO7 // GpioCtrlRegs.GPAPUD.bit.GPIO7 = 0; // Enable pullup on GPIO7 GpioCtrlRegs.GPAQSEL1.bit.GPIO7 = 0; // Synch to SYSCLKOUT InputXbarRegs.INPUT7SELECT = 7; // INPUT7 = GPIO7 ECap1Regs.ECCTL0.bit.INPUTSEL=7; // Select eCAP1 TO INPUT7 // // Enable GPIO outputs on GPIO8 - GPIO11, set it high // GpioCtrlRegs.GPAPUD.bit.GPIO8 = 0; // Enable pullup on GPIO8 GpioDataRegs.GPASET.bit.GPIO8 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 0; // GPIO8 = GPIO8 GpioCtrlRegs.GPADIR.bit.GPIO8 = 1; // GPIO8 = output GpioCtrlRegs.GPAPUD.bit.GPIO9 = 0; // Enable pullup on GPIO9 GpioDataRegs.GPASET.bit.GPIO9 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 0; // GPIO9 = GPIO9 GpioCtrlRegs.GPADIR.bit.GPIO9 = 1; // GPIO9 = output GpioCtrlRegs.GPAPUD.bit.GPIO10 = 0; // Enable pullup on GPIO10 GpioDataRegs.GPASET.bit.GPIO10 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 0; // GPIO10 = GPIO10 GpioCtrlRegs.GPADIR.bit.GPIO10 = 1; // GPIO10 = output GpioCtrlRegs.GPAPUD.bit.GPIO11 = 0; // Enable pullup on GPIO11 GpioDataRegs.GPASET.bit.GPIO11 = 1; // Load output latch GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 0; // GPIO11 = GPIO11 GpioCtrlRegs.GPADIR.bit.GPIO11 = 1; // GPIO11 = output // // Enable SPI-B on GPIO22 - GPIO25 // GpioCtrlRegs.GPAPUD.bit.GPIO22 = 0; // Enable pull-up on GPIO22 (SPICLKB) GpioCtrlRegs.GPAPUD.bit.GPIO23 = 0; // Enable pull-up on GPIO23 (SPISTEB) GpioCtrlRegs.GPAPUD.bit.GPIO24 = 0; // Enable pull-up on GPIO24 (SPISIMOB) GpioCtrlRegs.GPAPUD.bit.GPIO25 = 0; // Enable pull-up on GPIO25 (SPISOMIB) GpioCtrlRegs.GPAQSEL2.bit.GPIO22 = 3; // asynch input GpioCtrlRegs.GPAQSEL2.bit.GPIO23 = 3; // asynch input GpioCtrlRegs.GPAQSEL2.bit.GPIO24 = 3; // asynch input GpioCtrlRegs.GPAQSEL2.bit.GPIO25 = 3; // asynch input GpioCtrlRegs.GPAMUX2.bit.GPIO22 = 1; // GPIO22 = SPICLKB GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 1; // GPIO23 = SPISTEB GpioCtrlRegs.GPAMUX2.bit.GPIO24 = 1; // GPIO24 = SPISIMOB GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 1; // GPIO25 = SPISOMIB // // Enable SPI-A on GPIO16 - GPIO19 // GpioCtrlRegs.GPAPUD.bit.GPIO16 = 0; // Enable pull-up on GPIO16 (SPISIMOA) GpioCtrlRegs.GPAPUD.bit.GPIO17 = 0; // Enable pull-up on GPIO17 (SPISOMIA) GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0; // Enable pull-up on GPIO18 (SPICLKA) GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0; // Enable pull-up on GPIO19 (SPISTEA) GpioCtrlRegs.GPAQSEL2.bit.GPIO16 = 3; // asynch input GpioCtrlRegs.GPAQSEL2.bit.GPIO17 = 3; // asynch input GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3; // asynch input GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 3; // asynch input GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 1; // GPIO16 = SPISIMOA GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 1; // GPIO17 = SPISOMIA GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 1; // GPIO18 = SPICLKA GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1; // GPIO19 = SPISTEA // // Enable eCAP2 on GPIO24 // GpioCtrlRegs.GPAPUD.bit.GPIO24 = 0; // Enable pullup on GPIO24 GpioCtrlRegs.GPAQSEL2.bit.GPIO24 = 0; // Synch to SYSCLKOUT InputXbarRegs.INPUT8SELECT = 24; // INPUT8 = GPIO24 ECap2Regs.ECCTL0.bit.INPUTSEL=8; // Select eCAP2 TO INPUT8 // // Set input qualifcation period for GPIO25 & GPIO26 // GpioCtrlRegs.GPACTRL.bit.QUALPRD3=1; // Qual period = SYSCLKOUT/2 GpioCtrlRegs.GPAQSEL2.bit.GPIO25=2; // 6 samples GpioCtrlRegs.GPAQSEL2.bit.GPIO26=2; // 6 samples // // Make GPIO25 the input source for XINT1 // GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 0; // GPIO25 = GPIO25 GpioCtrlRegs.GPADIR.bit.GPIO25 = 0; // GPIO25 = input GPIO_SetupXINT1Gpio(25); // XINT1 connected to GPIO25 // // Make GPIO26 the input source for XINT2 // GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 0; // GPIO26 = GPIO26 GpioCtrlRegs.GPADIR.bit.GPIO26 = 0; // GPIO26 = input GPIO_SetupXINT2Gpio(26); // XINT2 connected to GPIO26 // // Make GPIO27 wakeup from HALT/STANDBY Low Power Modes // GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 0; // GPIO27 = GPIO27 GpioCtrlRegs.GPADIR.bit.GPIO27 = 0; // GPIO27 = input CpuSysRegs.GPIOLPMSEL0.bit.GPIO27=1; // GPIO27 will wake the device CpuSysRegs.LPMCR.bit.QUALSTDBY = 2; // Qualify GPIO27 by 2 OSCCLK // cycles before waking the device // from STANDBY // // Enable SCI-A on GPIO28 - GPIO29 // GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0; // Enable pullup on GPIO28 GpioCtrlRegs.GPAQSEL2.bit.GPIO28 = 3; // Asynch input GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1; // GPIO28 = SCIRXDA GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0; // Enable pullup on GPIO29 GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1; // GPIO29 = SCITXDA // // Enable CAN-A on GPIO30 - GPIO31 // GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pullup on GPIO30 GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1; // GPIO30 = CANTXA GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pullup on GPIO31 GpioCtrlRegs.GPAQSEL2.bit.GPIO31 = 3; // Asynch input GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1; // GPIO31 = CANRXA // // Enable I2C-A on GPIO32 - GPIO33 // GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0; // Enable pullup on GPIO32 GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 1; // GPIO32 = SDAA GpioCtrlRegs.GPBQSEL1.bit.GPIO32 = 3; // Asynch input GpioCtrlRegs.GPBPUD.bit.GPIO33 = 0; // Enable pullup on GPIO33 GpioCtrlRegs.GPBQSEL1.bit.GPIO33 = 3; // Asynch input GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 1; // GPIO33 = SCLA // // Make GPIO34 an input // GpioCtrlRegs.GPBPUD.bit.GPIO34 = 0; // Enable pullup on GPIO34 GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0; // GPIO34 = GPIO34 GpioCtrlRegs.GPBDIR.bit.GPIO34 = 0; // GPIO34 = input EDIS; } // // End of File //
The input sequence for the variable InputValue (GPIO12) will be [1 1 0 0 ] but the output sequence I observe for Boot from RAM mode is OutputValue = [0 1 1 0] but the output sequence observed for Boot from Flash mode is OutputValue = [1 1 1 0].
Is this expected behavior? What is the recommended workflow in these cases?
Thanks,
Aditya
Can you comment on this?
Hi Nima,
In the attached code, the InitSysCtrl function is called first which in turn should call the function InitFlash, if _FLASH is configured. This function I think will configure the required wait state as per the logic below.
//
// Set waitstates according to frequency
//
// *CAUTION*
// Minimum waitstates required for the flash operating at a given CPU rate
// must be characterized by TI. Refer to the datasheet for the latest
// information.
//
#if CPU_FRQ_200MHZ
Flash0CtrlRegs.FRDCNTL.bit.RWAIT = 0x3;
#endif
#if CPU_FRQ_150MHZ
Flash0CtrlRegs.FRDCNTL.bit.RWAIT = 0x2;
#endif
#if CPU_FRQ_120MHZ
Flash0CtrlRegs.FRDCNTL.bit.RWAIT = 0x2;
#endif
Thanks,
Aditya
Run through code, single stepping and make sure these lines get executed.
Nima
Hi Nima,
Yes I have stepped through these lines of code. The flash wait states configuration are executed properly.
Thanks,
Aditya
Aditya,
You are executing this in while (1) loop. How are you observing the value for OutputValue at different time ? Can you have four different variables for each assignment so that it is more clear ?
Regards,
Vivek Singh
Hi Vivek,
This is the while loop we have in the code.
while(1)
{
InputValue = 1;
if (InputValue == 1)
GpioDataRegs.GPASET.bit.GPIO12 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;
OutputValue = GpioDataRegs.GPADAT.bit.GPIO10;
DELAY_US(500000);
InputValue = 1;
if (InputValue == 1)
GpioDataRegs.GPASET.bit.GPIO12 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;
OutputValue = GpioDataRegs.GPADAT.bit.GPIO10;
DELAY_US(500000);
InputValue = 0;
if (InputValue == 1)
GpioDataRegs.GPASET.bit.GPIO12 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;
OutputValue = GpioDataRegs.GPADAT.bit.GPIO10;
DELAY_US(500000);
InputValue = 0;
if (InputValue == 1)
GpioDataRegs.GPASET.bit.GPIO12 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;
OutputValue = GpioDataRegs.GPADAT.bit.GPIO10;
}
In order to observe the behavior I put break points at 4 places.
1) At the first line of code inside the loop - InputValue = 1;
2) 3) and 4) At the 3 delays I have in the loop - DELAY_US(500000);
Every time I observe OutputValue and compare with the input value we set. This value varies when I do boot from Flash or RAM.
Yes if you want to replicate, you can change the code and have four different values of OutputValue as shown below to observe the behavior more clearly.
Uint16 OutputArray[4] = { 0, 0, 0, 0 };
while(1)
{
InputValue = 1;
if (InputValue == 1)
GpioDataRegs.GPASET.bit.GPIO12 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;
OutputValue = GpioDataRegs.GPADAT.bit.GPIO10;
OutputArray[0] = OutputValue;
DELAY_US(500000);
InputValue = 1;
if (InputValue == 1)
GpioDataRegs.GPASET.bit.GPIO12 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;
OutputValue = GpioDataRegs.GPADAT.bit.GPIO10;
OutputArray[1] = OutputValue;
DELAY_US(500000);
InputValue = 0;
if (InputValue == 1)
GpioDataRegs.GPASET.bit.GPIO12 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;
OutputValue = GpioDataRegs.GPADAT.bit.GPIO10;
OutputArray[2] = OutputValue;
DELAY_US(500000);
InputValue = 0;
if (InputValue == 1)
GpioDataRegs.GPASET.bit.GPIO12 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;
OutputValue = GpioDataRegs.GPADAT.bit.GPIO10;
OutputArray[3] = OutputValue;
}
Thanks,
Aditya
Hi Aditya,
Please confirm that GPIO12 is correctly configured as output by looking at DIR register value in CCS register view after configuration is done.
There is always some delay between output to input captured and it can take few cycles to update the value in input register after output value is set. To confirm this, can you insert some delay before reading the value (you can use DEALY function) and see if that helps in getting consistent value.
Regards,
Vivek Singh
Hi Vivek,
Yes all the pin are configured correctly. I have confirmed that in CCS.
Yes I do understand that there will be a delay of few cycles to update the value in input register after the output I set. And I have confirmed the same in my initial post. My question was specifically to understand the difference in the data read between Boot from Flash and Boot from RAM when delay is not used.
Thanks,
Aditya
Hi Vivek,
If we observe the sequence as explained above the different delays observed for transition from 1 to 0 and 0 to 1. But in data sheet I see that rise time and fall time for GPIO Output pins are same. (Chapter 5.8.6.1 GPIO - Output Timing, Table 5-21. General-Purpose Output Switching Characteristic)
Thanks,
Aditya
Hi Nima,
Other than the jumper wires connecting GPIO10 and GPIO12 I don't have any thing else connected.
Thanks,
Aditya
Were you able to resolve this? I don't have any further recommendations.
Vivek Singh Jason Whiles anything from your side on this topic?
Hi Nima,
I wanted to understand if this behavior is reproducible from TI side as well. If yes, is the behavior due to some software settings or hardware behavior?
If it is software then we can arrive at some solution or fix to solve the issue. (Looks like it is not as we verified different register combination in our discussions above.)
If it is hardware then at least this behavior can be documented for others.
I am ok to close this post. But it would be good to arrive at some conclusion for benefit of others in future.
Thanks,
Aditya
Aditya,
As you noted there is some transport delay between setting the output and seeing the results back on an input. For predictable testing here you should add a DELAY_US() statement before the OutputValue = GpioDataRegs.GPADAT.bit.GPIO10 . If these are back to back without delay then there will be variable results that could be influenced by many things.
Best regards,
Jason
Hi Aditya,
Besides the delay required, when setting and clearing GPIOs, it's recommended to use GPxSET and GPxCLEAR instead of GPxDAT. The read-modify-write that is performed in bitfield operations can have unintended consequences when GPxDAT is used to set and clear GPIOs.
Hi All,
Thanks for your suggestions on this issue. We can close this discussion.
Regards,
Aditya