This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: LAUNCHXL-F28379D eCAP and CLB

Part Number: LAUNCHXL-F28379D

Hey,

I'm using the F28379D launchpad and i have some problems ...

1- i use F28379D launchpad with the hardware support package on simulink ... but an uploading error is generated every time i try either to toggle an output pin with a frequency of 1 MHz or to set the sampling period of an input to to 1 usec. (notice the screenshot below)

2- How can I change the frequency of the counter of the ecap ? is it the syncIn input ? and if it is how to use it to change the frequency

3- Reagrding the CLB (configurable logic block) , where may I find all the possible assembly instructions that may be written on the program part of the HLC ?

Thanks