This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28388D: Can't Load CLA Application into Target device - Data Verification error

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE, TMS320F28379D

Tool/software: Code Composer Studio

Hello,

I am building a sample CLA application on TMS320F28388D controler. I am facing the below error when I tried to Load CLA program. The same issue is also present on the example programs present in the C2000ware folder: c2000\C2000Ware_3_02_00_00\driverlib\f2838x\examples\c28x\cla

CCS version: 10.0.0.00010

Compiler: TI v20.2.1.LTS

However, I was able to load the program and able to debug the CLA application on TMS320F28379D controller without any issues.

Please help to resolve the issue asap.

Thanks and Best Regards

Amulrass V