This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
In 'TMS320F28002x Microcontrollers Technical Reference Manual', Figure 17-51 DCxEVT1 Event Triggering shows there is no way to connect signal DCxEVT1.sync and signal DCxEVT1.
but they can be connected in Figure 13-50 of Tms320F28379s Delfino Microcontrollers Technical Reference Manual which marked with red circle.
The two figures is show as follow. Is there an error in the Figure 17-51?
The input to each of the OR gates is:
TZFRC and SYNC-DCEVT.
I will submit a request to fix the image.