This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: parallel boot mode for both CPU1 and CPU2 - GPIO selection

Part Number: TMS320F28379D

What is the recommended sequence of events when both CPU's are to bootload from parallel GPIO's? Should CPU1 finish its boot loading process, reassign GPIO's to CPU2 (GPIO69, 70, 63-58, 64, 65) and then send the IPC command to boot in parallel mode? Should the IPC command occur prior to assigning the GPIO's like the dual blink example? 

A detailed response will be highly appreciated. Thank you!