This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Greetings! I`m using a PGA input with gain=3 :
void initPGA(void) { PGA_setGain(PGA1_BASE, PGA_GAIN_3); PGA_setFilterResistor(PGA1_BASE, PGA_LOW_PASS_FILTER_DISABLED); PGA_enable(PGA1_BASE); } void initADCs(void) { // // Setup VREF as internal // ADC_setVREF(ADCA_BASE, ADC_REFERENCE_INTERNAL, ADC_REFERENCE_3_3V); ADC_setVREF(ADCB_BASE, ADC_REFERENCE_INTERNAL, ADC_REFERENCE_3_3V); ADC_setVREF(ADCC_BASE, ADC_REFERENCE_INTERNAL, ADC_REFERENCE_3_3V); // // Set ADCCLK divider to /4 // ADC_setPrescaler(ADCA_BASE, ADC_CLK_DIV_4_0); ADC_setPrescaler(ADCB_BASE, ADC_CLK_DIV_4_0); ADC_setPrescaler(ADCC_BASE, ADC_CLK_DIV_4_0); // // Set pulse positions to late // ADC_setInterruptPulseMode(ADCA_BASE, ADC_PULSE_END_OF_CONV); ADC_setInterruptPulseMode(ADCB_BASE, ADC_PULSE_END_OF_CONV); ADC_setInterruptPulseMode(ADCC_BASE, ADC_PULSE_END_OF_CONV); // // Power up the ADCs and then delay for 1 ms // ADC_enableConverter(ADCA_BASE); ADC_enableConverter(ADCB_BASE); ADC_enableConverter(ADCC_BASE); DEVICE_DELAY_US(1000); } void initCMPSS(void) { init_CMPSS_Modul(CMPSS1_BASE); } void init_CMPSS_Modul(uint32_t sellectedModul) { // // Enable CMPSS and configure the negative input signal to come from // the DAC // CMPSS_enableModule(sellectedModul); CMPSS_configHighComparator(sellectedModul, CMPSS_INSRC_DAC); CMPSS_configLowComparator(sellectedModul, CMPSS_INSRC_DAC); // // Use VDDA as the reference for the DAC and set DAC value to midpoint for // arbitrary reference. // CMPSS_configDAC(sellectedModul, CMPSS_DACREF_VDDA | CMPSS_DACVAL_SYSCLK | CMPSS_DACSRC_SHDW); CMPSS_setDACValueHigh(sellectedModul, CMPSS_HighValue); CMPSS_setDACValueLow(sellectedModul, CMPSS_LowValue); // // Configure digital filter. For this example, the maxiumum values will be // used for the clock prescale, sample window size, and threshold. // CMPSS_configFilterHigh(sellectedModul, 0x3FF, 32, 31); CMPSS_configFilterLow(sellectedModul, 0x3FF, 32, 31); // // Initialize the filter logic and start filtering // CMPSS_initFilterHigh(sellectedModul); CMPSS_initFilterLow(sellectedModul); // // Configure the output signals. Both CTRIPH and CTRIPOUTH will be fed by // the filter output. // CMPSS_configOutputsHigh(sellectedModul, CMPSS_TRIP_FILTER | CMPSS_TRIPOUT_FILTER); CMPSS_configOutputsLow(sellectedModul, CMPSS_TRIP_FILTER | CMPSS_TRIPOUT_FILTER); }
Here comes the problem! In this case when I read the PGA value the real voltage on the PGA1 pin is multiplied by 3 so for 0.17V I have result around 600. But It seems the CMPSS input takes the value before this multiplication, because if I have to set the DAC`s value very low. So I tried to change the input MUX value of the CMPSS input, but without any success. In my project I`m using all PGA inputs. What is procedure of changing the input of CMPSS?
Thanks!
I want to achieve this -> if the voltage is in a mid point for example 0.2V input(with gain=3) , both filters to have output 1 for example. If the voltage goes higher than comp1 dac value the output value to be 0. if voltage droped below comp2 value the same comp to have 0 on the output. Or something similar. Now I can`t achieve this. I don`t know why but the comparators don`t react properly to the input voltage. Are there any examples!
There are some muxes for configuring the CMPSS input. Have you taken a look at the Analog Subsystem chapter in the Technical Reference Manual? There are some block diagrams and tables explaining the different options. In driverlib, the corresponding functions are in asysctl.h and all start with "ASysCtl_selectCMP"
Whitney