Part Number: TMS320F28379D
Hi,
I have been trying to run an application from the internal flash memory on the TI 28379 Control Card. I changed the linker file to use the flash memory locations and defined _FLASH to enable memcpy. However I have been getting an error : " Break at address "0x3fe493" with no debug information available, or outside of program code" when I try to run the application. I am also changing the switch positions to get from flash for SW1. I am not sure if I am missing any other setup other than these two changes in setting up the run from Flash memory. Any suggestions will be really helpful.
Thank you,
Aditya