Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, BOOSTXL-POSMGR
Hello, I am using LAUNCHXL-F28379D with BOOSTXL-POSMGR to get the tamagawa encoder signal (t-fromat).
The TI reference program "tformat_f28379x_boostxl_posmgr_site2" is in use in the test.
However, some obnormal results are got.
1. No signal in expression window, the program is always waiting the "while(tformatData.dataReady != 1); " in the main.c while(1).
2. No clocking signal detected by the oscilliscope on PWM4B, GPIO63, GPIO64.
I am not sure, is the PWM4B controller by CLB or PWM4 registers? Why the PWM4 resisters are always as default when the program is running. At least the TBPRD should have been set, but not.
Any friends can help?
Best wishes
Lei