This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375D: CPU2 CLA issue

Part Number: TMS320F28375D


When adding new code to CPU2 flash, the CPU2 CLA not working properly. Moreover, other parts of CPU2 works properly. We have merged flash E, F, G, H, I and J to flashE. The memory configuration window doesn't show any memory overflow. Just removing the added new code, cause the CPU2 CLA work properly. Tried compiling the code also in different compilers from 16.9.6 to 18.1.8 in CCS 8.0 and 20.2.4 in CCS 10.2.0.

The CLA memory configuration and initialization routine is as below:

void CLA_configClaMemory(void)
{
    extern uint32_t Cla1funcsRunStart, Cla1funcsLoadStart, Cla1funcsLoadSize;

    EALLOW;

#ifdef _FLASH
    /*Copy over code from FLASH to RAM*/
    memcpy((uint32_t *) & Cla1funcsRunStart, (uint32_t *) & Cla1funcsLoadStart, (uint32_t) & Cla1funcsLoadSize);

#endif                                 /*_FLASH*/

    /*Initialize and wait for CLA1ToCPUMsgRAM*/
    MemCfgRegs.MSGxINIT.bit.INIT_CLA1TOCPU = 1;

    while (MemCfgRegs.MSGxINITDONE.bit.INITDONE_CLA1TOCPU != 1)
    {

    };

    /*Initialize and wait for CPUToCLA1MsgRAM*/
    MemCfgRegs.MSGxINIT.bit.INIT_CPUTOCLA1 = 1;

    while (MemCfgRegs.MSGxINITDONE.bit.INITDONE_CPUTOCLA1 != 1)
    {
    };

    /* Select LSxRAM to be the programming space for the CLA First configure the CLA
     * to be the master for LSx and then set the space to be a program block*/

    MemCfgRegs.LSxMSEL.bit.MSEL_LS4 = 1;              /*RAMLS4*/

    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS4 = 1;
    MemCfgRegs.LSxMSEL.bit.MSEL_LS5 = 1;              /*RAMLS5*/

    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS5 = 1;

    /* Next configure LSxRAM as data spaces for the CLA First configure the CLA
     * to be the master for LSx and the set the spaces to be Data blocks*/

    MemCfgRegs.LSxMSEL.bit.MSEL_LS0 = 1;              /*RAMLS0*/

    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS0 = 0;

    MemCfgRegs.LSxMSEL.bit.MSEL_LS1 = 1;              /*RAMLS1*/

    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS1 = 0;

    MemCfgRegs.LSxMSEL.bit.MSEL_LS2 = 1;              /*RAMLS2*/

    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS2 = 0;

    MemCfgRegs.LSxMSEL.bit.MSEL_LS3 = 1;              /*RAMLS3*/

    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS3 = 0;

    EDIS;
}

//CLA initialtization
void CLA_initCpu2Cla1(void) { /* Compute all CLA task vectors On Type-1 CLAs the MVECT registers accept * full 16-bit task addresses as opposed to offsets used on older Type-0 CLAs*/ EALLOW; Cla1Regs.MVECT1 = (uint16_t)(&Cla1Task1); Cla1Regs.MVECT2 = (uint16_t)(&Cla1Task2); Cla1Regs.MVECT3 = (uint16_t)(&Cla1Task3); Cla1Regs.MVECT4 = (uint16_t)(&Cla1Task4); Cla1Regs.MVECT5 = (uint16_t)(&Cla1Task5); Cla1Regs.MVECT6 = (uint16_t)(&Cla1Task6); Cla1Regs.MVECT7 = (uint16_t)(&Cla1Task7); Cla1Regs.MVECT8 = (uint16_t)(&Cla1Task8); /* Enable the IACK instruction to start a task on CLA in software * for all 8 CLA tasks. Also, globally enable all 8 tasks (or a subset of tasks) * by writing to their respective bits in the MIER register*/ asm(" RPT #3 || NOP"); Cla1Regs.MCTL.bit.IACKE = 1; Cla1Regs.MIER.all = 0x00FF; /* Configure the vectors for the end-of-task interrupt for all 8 tasks*/ /* PieVectTable.CLA1_1_INT = &CLA1_1_ISR; PieVectTable.CLA1_2_INT = &CLA1_2_ISR; PieVectTable.CLA1_3_INT = &CLA1_3_ISR; PieVectTable.CLA1_4_INT = &CLA1_4_ISR; PieVectTable.CLA1_5_INT = &CLA1_5_ISR; PieVectTable.CLA1_6_INT = &CLA1_6_ISR; PieVectTable.CLA1_7_INT = &CLA1_7_ISR; PieVectTable.CLA1_8_INT = &CLA1_8_ISR; */ /* Enable CLA interrupts at the group and subgroup levels*/ PieCtrlRegs.PIEIER11.all = 0xFFFF; IER |= (M_INT11); EDIS; }

The project's .map and .cmd files of CPU2 are attached for reference in map_cmd_files.zip file.

map_cmd_files.zip

Regards,

Amtech

  • Amtech said:
    When adding new code to CPU2 flash, the CPU2 CLA not working properly.

    Hi Amtech,

    Can you provide more information on how the CLA is failing to work?  Is a task starting but not completing? Or does the task never start?

    Immediately after the configuration of the CLA memory, if you view the CLA disassembly in CCS does it look like the code was copied over properly?  

    Try setting a breakpoint in the task.  Right after the configuration, start the task via software. Did (1) the task start? (2) can you step through the task to try and determine where things go wrong. 

    Were there any changes in the initialization? For example the order of initializing peripherals? If the CLA is initialized last it may not see the interrupt edge from a peripheral.

    Regards

    Lori