This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dual-axis motor control using FCL and SFRA On a Single C2000 MCU. (LEVEL 1)
I have searched the relevant post in e2e, and it says to remove the R20 on the BOOSTXL-3PhGaNInv, I have done.
but in the watch window I can see the variables changed . but no graph in the graph window.How should I do .and I have inspected the expressions that get out a New one named"Ctrlstate",what's the function?
also, I want wto ask if there is a new version of SPRACO3?
Below are my capture in the CCS.
Hi,
This appears to be a duplicate post. We'll close this thread and continue the discussion here.
I have solved the problem of no correct graph on the graph window. It because Now it has a variable of ctrlState, It shuld make to CTRL_RUN,Then all work well. Thank you so much!