Other Parts Discussed in Thread: TPS3702, LAUNCHXL-F280049C,
Hello.
TPS3702 seems to be used for LAUNCHXL-F280049C.
Is it possible to develop TMS320F280049C board without any reset IC such as TPS3702?
Is TPS3702 mandatory?
Regards,
U-SK
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
TPS3702 seems to be used for LAUNCHXL-F280049C.
Is it possible to develop TMS320F280049C board without any reset IC such as TPS3702?
Is TPS3702 mandatory?
Regards,
U-SK
Hi U-SK,
The F28004x has an internal BOR which will monitor VDDIO & put the device in reset if the voltage is outside of the recommended operating conditions.
As a result, for the F28004x, an external voltage monitor is generally not required.
However, some applications, such as ISO 26262 systems, may still require an external monitor.
Hopefully this helps!
Thank you,
Brett