Part Number: TMS320F28075
When I checked the error message of "XDS200 USB Debug Probe", I found the following description.
It seems that the voltage of "the TVRef pin" is abnormal. How many pins of TMS320F28075 is this pin specifically examined?
(about the "Error -180" message)
This error means the JTAG debugger is unable to sense the presence of a power supply voltage on the target - the TVRef pin.
Error connecting to the target:
(Error -180 @ 0x0)
The controller has detected a target power loss.
The user must turn-on or connect the power supply for the target.