Tool/software: Code Composer Studio
Hello,
I just received my new board mounted with TMS320F28051 and try to connect my XDS510LC to it through the JTAG connector. It is not possible to connect to it:
C28xx: Error connecting to the target: Error 0x80000220/-1135 Fatal Error during: Execution, OCS, Unrecoverable emulation error
I as well have the XDS100v2 which runs correctly.
Any idea why it is not running with the XDS510LC?
Additional information: I'm using CCS V7.3
Thanks in advance.
Steve