Part Number: TMDSHVMTRPFCKIT
In conjunction with operational testing of my three phase BLDC servo motors, I have the need to load test this motor which requires up to 13.5 Amps for a brief period (approx. 30 seconds to 1 minute in duration). My Question is; If I connect a External Isolating DC Power Supply with a max output rating of 350 VDC and 17 Amps, can I perform the load test up to 13.5 Amps with this TI Drive/Eval. Kit?
Ron Stewart