Other Parts Discussed in Thread: TMS570LS1114
Problem description:
when the PCB which employs TMS570LS0714 gets above 105*C the CAN comms are lost on power cycle(reset) and starts running only when temp drops below ~95*C. Either CAN comm IC shuts down and doesn't boot or CPU. When heating up just one of them at the time, the problem could not be reproduced
Tests revealed that possibly a certain IC or mixture of events may be causing CPU not to run properly or CAN comms to stop.
Tests were repeated with TMS570 development board but the problem did not occur. Later on same tests were carried out for a custom board that employs TMS570LS1114 and the problem did not occur.