Hi,
I have XDS110 standalone debug probe. Can i use this with TMS570LS12x HDK? Is there a application note or reference document?
Note: I know that the HDK itself has the on board debugger.
Thanks,-Dinesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have XDS110 standalone debug probe. Can i use this with TMS570LS12x HDK? Is there a application note or reference document?
Note: I know that the HDK itself has the on board debugger.
Thanks,-Dinesh
Hello Dinesh,
Yes, you can use XDS110 standalone debug probe.
Connector J4 of TMS570LS12x HDK is ARM 20pin JTAG Header where you can connect external JTAG probe.
At device web page ( www.ti.com/.../TMDSEMU110-U ) is shown that ARM20 adapter is supplied with the probe.
You can see TMS570LS12x Hercules Development Kit (HDK) user guide for details on J4 pinout and placement ( http://www.ti.com/lit/ug/spnu568a/spnu568a.pdf ).
Best regards,
Miro
Hi Miro,
None of the adapter provided with XDS110 can be used directly with J4 of TMS570LS12x HDK. Do we need to manually connect using wires?
-DInesh
Hi Mira,
Would you please suggest some link to find the converters between the tiny 20-pin ARM JTAG header to the big one on the TMS570LS12x HDK board?
Thanks,
Best Regards,
-Dinesh
Hello,
I am not aware whether spare adapters are in sale separate. You could contact your local TI reseller to ask about it.
Also check this page for different connectors pin-out:
The pin-out of HDK adapter can be find in HDK user guide and schematic that can be downloaded from product page:
Best regards,
Miro
Hi,
I bought the Olimax ARM 20 to 10 pin adaptor and it works fine.
Thanks,
Best Regards,
-Dinesh