Part Number: TMS570LS1227
Dear team,
I am debugging the TMS570LS1227 and currently I need to use a 1227 internal hardware to automatically turn off the PWM function. According to the manual description, user can self-turn off the HET2 PWM through GIOB[2].
The bottom layer of user debugging is automatically generated using HalcodeGen software, and the above functions are also configured in HalCodeGen software, as shown in the figure below
But it has not been able to turn off the PWM output of HET2 through the input level of GIOB[2].
Currently, the user’s approach is,
1. After the program is run, PWM has been outputting a PWM wave with a fixed duty cycle and period.
2. GIOB[2] is configured as input, and PINMUX is configured, as configured in the second picture,
3. Through an IO output to GIOB[2], or directly add a 3.3V or low level to GIOB[2], the PWM wave of HET2 has not changed.
Please help.