This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
Please let me check the RST/NMI/SBWTDIO pins.
Q1: Am I right in thinking that when the RST/NMI/SBWTDIO pin operates in reset mode (or NMI mode), it functions as an input and not as an output?
In general, I think the RST/NMI function works as an input. Also, I don't know the internal structure from the answer to the original question, but I believe it does not work as an output. However, since it is a dual-purpose pin with SBWTDIO function, it seems to work as input/output from the data sheet, so let me confirm this.
Q2: If the RST/NMI/SBWTDIO pin also functions as an output in reset mode, is there a case where the RST/NMI/SBWTDIO pin outputs Low?
Best regards,
O.H
Hello,
Yes, the RST/NMI pin always functions as a input pin. I would never expect it to drive the output low unless it was somehow damaged.
The question about SBW is interesting because SBWTDIO is bi-directional. I guess there is a pull-down circuit multiplex in if the JTAG interface is active. I can't recall this ever interfering with the RST line outside of programming, but I guess it's technically possible.
Are you seeing a specific issue of some sort?
Thanks,
JD
Hello DJ,
Thanks for the reply.
Yes, the RST/NMI pin always functions as a input pin. I would never expect it to drive the output low unless it was somehow damaged.
The question about SBW is interesting because SBWTDIO is bi-directional. I guess there is a pull-down circuit multiplex in if the JTAG interface is active. I can't recall this ever interfering with the RST line outside of programming, but I guess it's technically possible.
I understood.
Are you seeing a specific issue of some sort?
Related to the thread below, there is a problem with UART communication becoming unstable at high temperatures. (Data may not be observed on the communication line.)
According to the customer's investigation, sometimes no data is observed when a measurement device is connected to the communication line; when the RST/NMI pin is connected to the measurement device, it is fixed to Low, and shorting the RST/NMI pin to VCC restores the device.
We have not been able to identify a clear cause, and since we are checking the frequency response of the DCO and the processing and operation of the RST/NMI pins. This is why I asked this question.
Best regards,
O.H
**Attention** This is a public forum