This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553: Interface communication error with MSP430G2553

Genius 9880 points

Part Number: MSP430G2553
Other Parts Discussed in Thread: MSP-FET

Hi,

Good day.

Customer is encountering interface communication error with MSP430G2553. Below is the details.

"

I am facing problem while uploading the code? getting error as MSP430: Error Initializing : interface Communication error?

Heres my connection

JTAG pin 2 (VCC_TOOL) if MSP-FET powered, or JTAG pin 4 (VCC_TARGET) if externally supplied, to VCC

JTAG pin 9 (GND) to GND
JTAG pin 8 (Test/Vpp) to SBWTCK
JTAG pin 1 (TDO/TDI) to SBWTDIO

I am using MSP430G2553 ic . using thsi 2 wire method

https://www.ti.com/lit/ug/slau278ah/slau278ah.pdf#page=21

"

Thank you in advance.

Regards,
Maynard

  • Hi Maynard,

    You are looking at the correct documentation, but you also need to connect the JTAG !RST pin. The section "Signal Connections for In-System Programming and Debugging" states that the connection to this pin is required for devices that support 2-wire JTAG communication, even if you're using the 4-wire JTAG communication mode.

    Furthermore, make sure you're following Figure 2-2 for 2-wire JTAG.

    Regards,

    Urica Wang

**Attention** This is a public forum