Other Parts Discussed in Thread: ENERGIA
I've been trying trying to program MSP430 using MSP-FET but everytime I try to program, I get an error message that says 'MSP430: Error connecting to the target: Unknown device'. I have connected a wire with bug strip on one side and with JTAG on the other side that gets connected to the JTAG port on the circuit board.
Did not see this issue earlier but suddenly this error has started to show up. There is no change in the hardware so do not anticipate any issue on the HW side. I have tried programming on multiple boards but no luck. I would like to add, I have on an onboard power supply in the form of Li-Ion battery and there is power LED that starts blinking when I try to program. If I remember correctly, earlier when the programming worked the power LED remained solid the entire time. Not sure if blinking LED is some of indication here. Any help would be greatly appreciated!