Other Parts Discussed in Thread: UNIFLASH
Hello,
Currently i am facing the issue while having the AC metering using EVM430i2040s.
1) I made both connection for flashing the code and actual AC metering setup as per given in the technology guide.
2)First i took the pre saved example of the EVM430i2040s 50Hz and loaded the same on EVM through Uniflash.
3) Now after connecting the load to the EVM, i have also connected the power analyzer for accuracy purpose but in actual i am getting only 86-87W active input power also IRMS is only 0.34 A on power analyzer. But in GUI i am getting following values which are too high than expected,
VRMS | 220.85 |
IRM | 3.012 |
VPEAK | 311.532 |
IPEAK | 4.260 |
Phase Angle | 2.43 |
Power Factor | .99 |
frequency | 50 |
Active power | 453.363 |
Reactive power | 19.07 |
Apparent Power | 453.67 |
What should i done to get a correct values.
4) Also please provide the solution for how to provide the correct values for getting accurate values.
5) What should be done for erasing flash memory through Uniflash.
P.S. Please provide the solution As soon as possible.
Thanks & Regards
Gautam