Part Number: MSP430F5529
I WANT TO READ DATA FROM SPECIFIC 0X03 REGISTER OF I2C SLAVE MODULE USING MSP430F5529 BUT INSTEAD OF 16 BIT DATA WITH ACKNOWLEDGE I COULD ONLY GET 8 BIT DATA WITCH NACK.MY CODE
#include <msp430.h>
char Data_In=0;
unsigned char RXByteCtr;
unsigned char *PRxData;
volatile unsigned char RxBuffer[128];
void main(void)
{
volatile int i;
WDTCTL = WDTPW + WDTHOLD; // Stop WDT // P1.0 output
P3SEL |= 0x03; // Assign I2C pins to USCI_B0
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode
UCB0CTL1 |= UCSSEL_2; // Use SMCLK
UCB0BR0 = 12; // fSCL = SMCLK/12 = ~100kHz
UCB0BR1 = 0;
UCB0I2CSA = 0x40; // Slave Address is 048h
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
UCB0IE |= UCTXIE;
UCB0IE |= UCSTPIE + UCSTTIE + UCRXIE;
volatile int c=1;
__enable_interrupt();
while(1)
{
RXByteCtr = 2;
UCB0CTL1 |= UCTR + UCTXSTT;
while (UCB0CTL1 & UCTXSTP);
UCB0CTL1 &=~UCTXSTP;
UCB0CTL1 &=~UCTR;
UCB0CTL1 |=UCTXSTT;
while (UCB0CTL1 & UCTXSTP);
UCB0CTL1 &=~UCTXSTP;
}
}
#pragma vector = USCI_B0_VECTOR
__interrupt void USCI_B0_ISR(void)
{
switch(UCB0IV){
case 0x0A:
RXByteCtr--; // Decrement RX byte counter
if (RXByteCtr)
{
*PRxData++ = UCB0RXBUF; // Move RX data to address PRxData
if (RXByteCtr == 1) // Only one byte left?
UCB0CTL1 |= UCTXSTP; // Generate I2C stop condition
}
else
{
*PRxData = UCB0RXBUF; // Move final RX data to PRxData
__bic_SR_register_on_exit(LPM0_bits); // Exit active CPU
}
break;
case 0x0C:
UCB0TXBUF = 0X01;
break;
default:
break;}
}