I intend to use this Launchpad as a peripheral on a PC using Serial Communication. If I don't have CCS installed is there a way to install drivers to allow serial communication with the back-channel UART?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I intend to use this Launchpad as a peripheral on a PC using Serial Communication. If I don't have CCS installed is there a way to install drivers to allow serial communication with the back-channel UART?
Hi Keith,
I believe you should be able to install those driver via CCS cloud(without installing CCS).
BR,
Leo
Hi Keith,
The TI Cloud Agent will get installed when using CCS Cloud. According to the Overview in the TI Cloud Agent user's guide, device-specific support files are downloaded as needed to minimize the size of the installation footprint. The TI Cloud Agent should install drivers for the common debuggers and allow the back-channel UART to be used. Otherwise, you may need to import a project for your device into CCS Cloud and download/debug to install any other files that may get used by the device and/or debugger.
Thanks, I want this to be installed on computers that have no need for CCS, so I think I will just get a USB-Serial adapter with an FTDI chip. At one time I thought there were separate driver packages.
Hi Keith,
I'll have to try the USB drivers link. Before installing anything on my personal PC, I just plugged in a G2ET LaunchPad and was able to transmit data from a serial terminal (but not receive it) through the back-channel UART. My setup:
Personal PC --> USB cable --> G2ET LP --> U105 TX pin (RXD<<) on LP --> RX pin on TTL-to-USB serial adapter --> Work PC
Here's what the LaunchPad looks like in Device Manager without installing anything.
I used COM5 (first one) as the Application (back-channel UART) interface.
So you bypassed the EZ_FET on the G2ET launchpad/
No, I went through it. I updated my crude setup diagram above to be more clear.
Okay, I switched to a FR2311 LaunchPad (sorry, was using G2ET earlier). Without installing anything, I was able to get both TX and RX to work using the back-channel UART on the FR2311 LaunchPad. I remembered that the G2ET LaunchPad has SW and HW UART support, depending on the jumper orientation on the isolation jumper block, and I think that explains why only TX worked for me.
As far as installations, I only have the Energy Measurement Design Center installed on my personal PC. That's the only thing in the C:\ti folder. I didn't find anything else that would have installed drivers.
Edit: I did notice that the Debug port enumerated first rather than second for this LaunchPad. It was second for the G2ET LaunchPad, so it doesn't seem like the order is consistent.
Thanks. I'll try. It can't hurt. I would not be surprised in the EMDC did not install drivers. Doesn't it use USB-Serial to talk to the GUI?
Hmm, I don't think EMDC installs any drivers, specifically because our Design Center framework relies on USB HID bridges to avoid drivers that are typically required for USB CDC devices. Unfortunately, I don't have any more PCs without installed drivers. Hopefully, you get the same result as I did on a fresh PC. Let us know what you find out.
**Attention** This is a public forum