This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5889: Technical issues

Part Number: MSP430FR5889

Hi team,

I got a question from customer.

"As I have been writing regarding the issues in PORT1, where one pin9 (port 9.0)designated as analog input, while other 7 pins as DIGITAL OUTPUT,the ADC reading is going wrong. The ADC READING GOES WRONG when communication in PORT 4(PORT 4.2Tx&4.3Rx ) is initiated.All the power supplies are isolated at the source itself with only ONE POINT INTERCONNECTION as needed.The communication port is driving RS485 through an ISOLATED POWER SUPPLY and the digital isolator (MAX14932 DAWE+)drawing very small current .wHEN THIS IS SWITCHED off ADC READING becomes normal.."

MSP430FR5889IPM_MODIFIED DESIGN.pdfMSP430FR5889IPM_OLD DESIGN.pdf

Thank you very much for your help.

Best regards,

**Attention** This is a public forum