This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what's the difference AVCC1 and AVCC2 in msp430fr5994? Are they having the same function? Do i need to connect all pins of them?
Hi Gaosheng Liu,
Is this the proper device? I was looking at the datasheet for the device and there is no mention of an AVCC2, but there is a DVCC1/2/3 and an AVSS1/2/3. If this is the right device were you asking about the DVCC or the AVSS then?
Regards,
Luke
Hi Luke,
Yes, There are AVCC1/ AVSS1, AVSS2, AVSS3/AGND, and DVCC1, DVCC2, DVCC3/AVSS1, DVSS2, DVSS3/DGND.
Hi Luke,
I don't understand the difference between them yet. As the questions describe up.
Best,
Gaosheng
Hi Gaosheng,
The DVCC supplies all the digital modules and the AVCC supplies the analog modules. AVSS and DVSS are needed for ground. I would suggest just connecting all of them to the appropriate values. You can connect all the DVCC to the same source. And all the ground to the same ground.
Regards,
Luke
**Attention** This is a public forum