Part Number: MSP430G2553
Hello everyone,
Greetings!!!
My task is to reset the microcontroller if it's halted, for that, I am using a watchdog timer,
I am setting the watchdog time period as 1sec and am clearing WTD every 200ms for that I am using a timer so that the WTD won't reset every 1sec,
I wrote code, I wish to check the program so I added while(1);, the program halted here, the WDT is not resetting the microcontroller,
my program holds on while(1);, what's the problem, am I doing anything wrong? please guide me on how to solve it. I have mentioned my code below for your reference.
#include "msp430g2553.h"
unsigned int Timer1ms=0;
unsigned int count=0;
void Timer_Init();
void main(void)
{
WDTCTL = WDTPW + WDTHOLD;// Stop the WDT to prevent reset // Count value for delay
Timer_Init();
WDTCTL = WDT_ARST_1000; // 1 sec watchdog interval
while(1)
{
// WDTCTL = WDT_ARST_1000;
count++;
if(count>5000)
{
while(1);
count=0;
}
}
}
void Timer_Init()
{
DCOCTL = CALDCO_8MHZ;
BCSCTL1 = CALBC1_8MHZ;
TA0CCTL0=CCIE;
TA0CTL=TASSEL_2+MC_1+ID_3;//SMCLK, Up mode, Divider -->1
TA0CCR0=999;//from above calculation
_BIS_SR(GIE);//off CPU until interrupt occurs
}
#pragma vector=TIMER0_A0_VECTOR
__interrupt void TIMER0_A0_ISR(void)
{
Timer1ms++;
if(Timer1ms>=200)
{
WDTCTL = WDTPW + WDTHOLD + WDTCNTCL;// Stop WDT
WDTCTL = WDT_ARST_1000; //again 1sec reload
Timer1ms=0;
}
}
Thanks in advance!!
Regards,
Aravinth K.