Other Parts Discussed in Thread: MSP430F5438A
Dear All,
Our device is turning OFF when reset is initialized by the WDT TIME_OUT expiration.
In our design we have used MSP430F5438A controller. We are implementing the Watch dog function to perform controlled restart after device hangs due to some unknown reasons. Now I am verifying the functionality to restart our device after 16 sec.
I have added the following line of code in our code to restart our device after 16 sec.
WDTCTL = (WDTPW+WDTCNTCL+WDTSSEL0+ 0x0003);
But I am facing issue when the device is turned OFF after updating the firmware, and then Turned ON. I have observed with the help of LED indication that the device is restarted after 16 sec, after after few initial HW initialization device is getting turned OFF.
The WDT functionality works perfectly fine during the updating the firmware using Code composer studio while debugging. The device is restarting at regular interval of 16 sec every time.
I am unable to understand what could be the issue is?.
Please reply as ASAP.
Thanks and Regards.
Bhairu