This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5519: Micro SD Card Connection - DM3D-SF

Part Number: MSP430F5519

Hello,
I want to store data with micro sd card in my circuit, but I couldn't find a specific sd card connection image for MSP430. I adapted my own micro sd card according to the only image I could find. Can it work smoothly as a result of the connection I made?

Here is my SD card connection:
CLK -> SCLK
DAT0 -> MISO + 50K TO 3V3
DAT1 -> 50K TO 3V3
DAT2 -> 50K TO 3V3
CD/DAT3 -> CS + 50K TO 3V3
CMD -> MOSI + 50K TO 3V3
VDD -> 3V3
SWA AND SWB -> NULL
SHIELD -> NULL
VSS ->GND

I would be very grateful for your answers, thank you.

**Attention** This is a public forum