Other Parts Discussed in Thread: MSP430F2013, MSP-FET, UNIFLASH
(Almost too embarrassed to state that title, as its featured countless times since the MSP430-FET arrived.)
My problem:
I have used the MSP430F2013 and its tiny cousins for years & have seen the infamous MSP-FET message "Error connecting to the target: Unknown device" a few times as well, and have pretty much worked out how to get around it for that chip. A recent upgrade required a couple more ports though, so the 20 pin MSP430G2452 was pressed into service. I expected to drop that chip into the circuit as an almost direct replacement. The SBW should have been almost exactly the same. To head off any communication issues I did not load the 2n2 reset capacitor (C1 below) for debugging with the MSP-FET, but to no avail.
What have I tried?
- CCS11 operating in Ubuntu 20.04 was installed to replace CCS10
- tried Uniflash 6.1 but it could not automatically detect the device
- SBW connections to the MSP430G2452 were checked again and confirmed
- 3.44Vcc is applied externally to the custom board & the MSP-FET is connected to suit - in the same manner as with previous MSP430F2013 projects (no change)
- With the MSP-FET connected, but not communicating, pin 16 (sbwtdio) is at 3.44V & pin 17 (sbwtck) is at 1.26V [I expected higher]
- I haven't put the oscilloscope on it yet
- I haven't tried to upgrade the MSP-FET firmware, and CCS11 hasn't attempted to do this for me. (I am not sure if this is necessary)
There is a 10uF filter capacitor at the output of an LT3012 voltage regulator that is not shown
Do you have any suggestions?