MSP430G2333 can this be used in RTC project,
Can i connect an external crystal of 32768Hz and use timer to keep real time ,and can it wake up from LPM3.5 with timer interrupt and pin interrupt.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can i connect an external crystal of 32768Hz and use timer to keep real time ,and can it wake up from LPM3.5 with timer interrupt and pin interrupt.
Hi prashanth k b,
MSP430G2333 does not have LPM3.5. LPM4 is the lowest power mode that device offers. The device can wake from a GPIO in LPM4. However LPM4 disables all the clocks which means you will not be able to run the timer in LPM4. If you use LPM3 (which has ACLK running) you can wake from a timer interrupt.
Evan
Thanks you Evan for the info,so MSP430G2333 can be used as RTC ,while LMP 3 will consume 1.2 u amp as compared to LPM3.5 0.72uamp.
I'm not sure I understand your comment. LPM3.5 doesn't exist for this device. Table 5-6 in the datasheet has the information you need:
Regards,
Evan
**Attention** This is a public forum