MSP430f5436 MICRO CODE SPACE
Can the msp430 compiler generate fully relocatable code for programs located above 64K in flash memory? We need a program linked to run in Bank 1 to be able to run in Bank 2 of main code memory. Is there any way to tell the compiler or linker to use relative addressing only and not use 20-bit absolute addressing?
Thanks