Other Parts Discussed in Thread: CC3200, CC1352P7
Hi,
I have LP-CC1352P7-4 launhpad, for which i have mounted BOOSTXL-AUDIO, and made connection changes as per I2S echo example given
https://dev.ti.com/tirex/explore/node?node=ADgQkBnE1H5pEBm2TFEl3A__fc2e6sr__LATEST
There are bending of pins recommended as below :
CC3200 Audio BoosterPack
- The BoostPack’s
DIN
signal pin is not compatible with this LaunchPad. Use one of the following modification(s) to enable the CC3200 Audio BoosterPack’s usage with the i2secho example. - Bend down the two pins below
DIO30
. Additionally bend downDIO28-30
. Be sure that the bent pin(s) do not make contact with the IC or any other component, bend them enough to make sure they don’t connect to the CC3200 Audio BoosterPack. - Attach the CC3200 Audio BoosterPack to the LP_CC1352P7_4
Till this portion, i got it connected , but below ones i am unable to find and locate them.
- Run jumper wires between the following pins on the CC3200 Audio BoosterPack:
- DIN:
P3.3
andP3.9
- DOUT:
P3.4
andP3.10
- BCLK:
P3.5
andP3.8
- FSYNC/WCLK:
P4.9
andP3.7
- DIN:
- See Audio BP User Guide, Figure 2-1 for information on where these pins are located.
- See below for a diagram.
I tried flashing I2S echo audio example, i am unable to get echo back of audio .
Can you please help.