Part Number: EVM430-I2040S
I want to measure energy of a single phase AC load using CT. Maximum load current measure up to 32A. If replace shunt with CT and measure maximum 32A load current then what changes need in circuit destine.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EVM430-I2040S
I want to measure energy of a single phase AC load using CT. Maximum load current measure up to 32A. If replace shunt with CT and measure maximum 32A load current then what changes need in circuit destine.
Hi Harshal,
Give me some time to look into this, will respond again soon.
regards,
Henok
Hi Harshal,
So since its a bit of an open ended question I will first provide you some blogs/technical articles to narrow down.
Single Phase and DC Embedded Metering using MSP430I2040
overcoming disadvantages of using shunt
Is there are particular reason why you are replacing the shunt with current transformer?
regards,
Henok
We want to use it single phase AC energy with max current up to 32A and CT is used as per client requirement.
How can I implement it please suggest.
Hi Harshal,
I will try to find if we have an implementation guide for this case.
In the meantime we do have similar app notes for other families.
Checkout:
regards,
Henok
**Attention** This is a public forum