Other Parts Discussed in Thread: MSP430F2274, CD4555B
Hi guys, I'm new in this area and i am desperately need help as i am really stuck here. I'm supposed to display the 4 digits which the first digit of the led showing "1" followed by "2" then "3" and "4". Im supposed to set a timer inside and making it run very fast. So fast that my 4 digit 7 segment display is showing 1,2,3,4 instead of 1|0|0|0 , 0|2|0|0, 0|0|3|0, 0|0|0|4 I need the codings urgently and if can please help me up. thanks a million. Im using msp430f2274 to display the 4 digit 7 segment display. Thank you very much.