Hello everyone. I'm trying to process some data using the MSP430FR4133 EVM, and i'm getting this issue where my variables are being written to the same register. This snippet of code i'm taking in some dummy array of 8 bit values, combining them into one 16 bit value, and then dissecting them into an exponent (bits 15-12) and a mantissa (bits 11-0). Whenever i run the code the exponent variables shares its value with the "value" variable. I looked and they using the same register as their address. How can I specify them not to be this way?