Other Parts Discussed in Thread: CODECOMPOSER
I've installed CodeComposer to re-compile an existing firmware for the MSP430FR5989IPM to determine the amount of FRAM and RAM used. The FRAMUtilities_03_10_00_10_setup has been run and its files are on this Windows 11 workstation. Yet all attempts to Build the code gives: "Product com.ti.mcu.msp.framutilities v3.10.0.10 is not currently installed and no compatible version is available. Please install this product or a compatible version."
How do I get CodeComposer to recognize the FRAMUtilities?
Re-installing FRAMUtilities 03_10_00_10 had no effect – the same error happens, and the compilation fails. The FRAMUtilities files were installed in the default location of C:\ti\msp430\FRAM-Utilities_03_10_00_10 while CodeComposer is at C:\ti\msp430\ccs and the project being compiled is at C:\Users\JHorn\workspace_v12\(Project name).
I really need to get this working to migrate the code to another of your MSP430 family. Your help is most appreciated!