Hi Team,
There's an issue from the customer need your help:
I'm using MSP-TS430PN80USB to connect to PC by USB(usb power jumper has been set , mcu digital and analog pin have voltage). Win7 system has no react. Installed uniflash_sl.8.1.1.4146. Press usb bsl(S3) button, then
system popped '"A device was found that the system does not recognize'. If you press and hold it, system will keep popping up.
Am I overlooked something? I've checked the circuit and no problem, the XT1 32.768 crystal is not installed. XT2 4MHz crystal is installed.
Could you help check this case?
Thanks & Regards,
Ben