This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2355: eUSCIB UCGLIT timings

Part Number: MSP430FR2355

Hello,

I had a customer point out to me that the deglitch times for UCGLITx are defined in the datasheet as follows:

However the comments in the MSP430FR2355.h include file suggest some different values:

/* UCA0CTLW1 Control Bits */
#define UCGLIT                           (0x0003)        /* Deglitch time */
#define UCGLIT_L                         (0x0003)
#define UCGLIT0                          (0x0001)        /* Deglitch time */
#define UCGLIT0_L                        (0x0001)
#define UCGLIT1                          (0x0002)        /* Deglitch time */
#define UCGLIT1_L                        (0x0002)
#define UCGLIT_0                         (0x0000)        /* Approximately 2 ns (equivalent of 1 delay element) */
#define UCGLIT_1                         (0x0001)        /* Approximately 50 ns */
#define UCGLIT_1_L                       (0x0001)
#define UCGLIT_2                         (0x0002)        /* Approximately 100 ns */
#define UCGLIT_2_L                       (0x0002)
#define UCGLIT_3                         (0x0003)        /* Approximately 200 ns */
#define UCGLIT_3_L                       (0x0003)

Which timings are the ones the customer should go with?

Munan

**Attention** This is a public forum