Part Number: MSP430FR2476
Good morning everyone,
I am not entirely new to the MSP430 world, and I have a decent experience as embedded firmware programmer. Driverlib is something new from my previous experience with MSP430, and
I find it an excellent tool....once I will be able to make it work.....
I just added this so that once the problem will be solved I will look even more like a fool :).
My problem is that I need to develop a very simple project in which a sensor is connected via I2C to an MSP430 device, and the CPU periodically reads the value.
So far so good....I thought. So, I ordered 2 development kits of MSP430, I read the driverlib documentation and I decided to use the I2C example as a reference. The MSP used in the example are
the FR4133, but I thought the difference was just in the port and pins configuration.
To make the long story short, I am struggling since a few days to have the I2C working! No matter what I try, I always have nothing on my logic analyser, and this is driving me crazy!
I am now in the easiest configuration I can imagine: I have the development board connected via USB to the PC, I have my logic analyser connected to the Eusci_B0 pins which are supposed
to work as I2C (1.3 and 1.2) and I run the basic code that follows
#include "driverlib.h"
volatile uint8_t transmitData;
int main(void) {
WDT_A_hold(WDT_A_BASE);
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P1,
GPIO_PIN2 + GPIO_PIN3,
GPIO_PRIMARY_MODULE_FUNCTION
);
PMM_unlockLPM5();
//Initialize Master
EUSCI_B_I2C_initMasterParam param = {0};
param.selectClockSource = EUSCI_B_I2C_CLOCKSOURCE_SMCLK;
param.i2cClk = CS_getMCLK();
param.dataRate = EUSCI_B_I2C_SET_DATA_RATE_400KBPS;
param.byteCounterThreshold = 1;
param.autoSTOPGeneration = EUSCI_B_I2C_NO_AUTO_STOP;
EUSCI_B_I2C_initMaster(EUSCI_B0_BASE, ¶m);
//Specify slave address
EUSCI_B_I2C_setSlaveAddress(EUSCI_B0_BASE,
0x48
);
//Set in transmit mode
EUSCI_B_I2C_setMode(EUSCI_B0_BASE,
EUSCI_B_I2C_TRANSMIT_MODE
);
//Enable I2C Module to start operations
EUSCI_B_I2C_enable(EUSCI_B0_BASE);
transmitData = 1;
while (1)
{
//Send single byte data.
EUSCI_B_I2C_masterSendSingleByte(EUSCI_B0_BASE,
transmitData
);
//Delay until transmission completes
while (EUSCI_B_I2C_isBusBusy(EUSCI_B0_BASE)) ;
//Delay between each transaction
__delay_cycles(50);
//Increment transmit data counter
transmitData++;
}
return (0);
}
I would expect to see something on the logic analyser, but the signals are never moving (and yes, I double checked that the analyser works....it does).
So, my question is....what is wrong here? I already tried the example codes (singleTX, multipleSlaves, and so on), I already tried a second board, I tried all the possible clock system configurations and clock sources.....always the same issue. The out_of_box example works fine, and I am able also to blink on board leds and to move the pins high/low.....but the I2C does never work!
Please, someone point me to the right direction to understand this weirdness.....what am I missing??