Hello Team,
Posting on behalf of my customer:
I am using a MSP430F23X powered at 3.3V, with 3.3V outputs. However, i have a number of inputs that are 1.8V. Will this MC accept 1.8V inputs in this setup?
The datasheet is unclear, as it states for a VCC of 3V, there is a MIN & MAX for positive-going input threshold voltage. Usually, there's just a minimum, and when the input voltage exceeds that minimum, it counts as a 1. This is especially true of schmitt-triggers. I don't know what to make of this "range." A 1.8V input signal falls smack in the middle of this range. Does it need to exceed the MAX of 2.25V ?
Regards,
Renan