Hi team,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Hi Kokila,
You can find related information in the UG chapter 5.2.12 UCS Module Fail-Safe Operation.
For current consumption information, please refer to the device datasheet chapter 8.4 and 8.5.
Best regards,
Cash Hao
Hi
Thanks for the reply.
UCS module fail-safe operation is mentioned in userguide, but how to verify that our varient has that support? Or Does all the MSP430 series have the support? In datasheet I couldn't find anything related to the Fail-safe operation.
Hi
When referred in the userguide, came to know that XT1,XT2,REFO are required for fail safe mechanism. when checked in datasheet of MSP430F5358 all these three are available. can i conclude that the fail safe mechanism is available in the MSP430F5358?
Regards
Kokila K
Hi,
Yes. The fail safe mechanism is available in the MSP430F5358.
Best regards,
Cash Hao
Thank you. And also i am having a doubt like when i have enabled XT2 and it got failed then the MCU will switch to REFO or XT1(in code i have given nothing regarding XT1). 32.678Khz is connected between Xin and Xout. Let me know what will happen in this scenario.
**Attention** This is a public forum