Other Parts Discussed in Thread: TLV320DAC3203
Hi dear people,
I have a question related to the clock system of the MSP430FR2633.
I understand, by clocking the device using the VLO I can go under to LPM4 and still be able to use Captivate.
This, because Captivate uses its own high frequency oscillator. Am I correct?
The question is, can I feed the TLV320DAC3203 with a clock comming from the MSP, while these is in LPM4?
Greetings from Spain, with 39° C at almost midnight!
Gustavo