Hi Team,
There's an issue from the customer need your help:
Hello, our test medium is air, the instrument sets the flow rate 6m³/h, and the temperature test is carried out in this environment.
At room temperature 20-25 °C, the instantaneous flow rate detected by the gas meter is about 6m³/h, and the consistency is good. However, at a high temperature of 50 °C, the instantaneous flow rate detected by the gas meter is unstable and fluctuates greatly. What could be the cause?
Thanks & Regards,
Ben