Other Parts Discussed in Thread: ADS1298
Dear All,
Good morning, I am working on a new product in which I have the MS430FR6989 microcontroller as the center of the design, with two external 32768hx crystals in LX and one 16Mhz in Hx. In euscib0 configured as spi it is connected to the ads1298, and in uscia0 configured as uart, there is a module with a wifi connection.
The query is, there are libraries available (*.c and/or *.h), both for serial communications (uart, spi, i2c), and for communication with database systems such as MySQL or Firebase, clock configurations, pinouts etc. ?! This is because, when developing, it allows shortening development and testing times.
I hope you can help me ....
Thank you so much!
Greetings